Nodejs do_compile fails.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nodejs do_compile fails.

1,165件の閲覧回数
MginoM
Contributor I

Hi all,

I'm a bit new to creating images so I'm running into multiple errors which I have been resolving.  Now, I have run into an error that I can't resolve.

Host Machine is running Ubuntu 20.04

Target machine is imx8 mini.

distro is fsl_imx_xwayland

machine is imx8mevk

image is imx_image_multimedia.

I was able to create the image successfully without nodejs.

When I try to create same image but adding IMAGE_INSTALL:append = " nodejs" to local.conf the compilation fails with exit code "1".  Same error if I attempt to compile nodejs recipe by itself.

the bb file indicates that the nodejs version is 16.11.1.

Any ideas on how to resolve this issue?

thanks,

 

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)