No u-boot console when loaded from DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No u-boot console when loaded from DDR

1,945 Views
mohamed-ali_fod
Contributor I

Hi,

I am using  "JLinkExe -device CORTEX-A9 -JTAGConf -1,-1  -if JTAG -speed auto -CommandFile uboot.jlink"
to load the uboot to the memory (attached is the script and the uboot binary), but I am still not able to get u-boot traces from the console. The u-boot was compiled with following config:

CONFIG_BOOTDELAY=5
# CONFIG_DISABLE_CONSOLE is not set
The uboot.imx.bin was successfully loaded as mentioned below:
J-Link>mem32 0x177ff000,9
177FF000 = 402000D1 17800000 00000000 177FF42C
177FF010 = 177FF420 177FF400 00000000 00000000
177FF020 = 177FF000
J-Link>mem32 177FF42C,9
177FF42C = 00000000 00000000 00000000 00000000
177FF43C = 00000000 00000000 00000000 00000000
177FF44C = 00000000
IVT - start = 177FF000
IVT - entry = 17800000
Any idea?
Thanks.
0 Kudos
Reply
3 Replies

1,863 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mohamed

reason may be that memory is not working at all, one can try

to test it with baremetal sdk test (folder  /..apps..tests/ddr_test.c), debugger scripts in

../tools, "1.1.0_iMX6_Platform_SDK.zip" found on link SMP Enable in IMX6 

Check signals with oscilloscope, use IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,863 Views
mohamed-ali_fod
Contributor I

Hi Igorpadykov,

Thank for you reply but I don't think that is a memory issue because I am able to write/read data correctly as I mentioned in my first post, if it was a memory issue I should not have access to the memory for write or read operations.

Before loading uboot I did the configuration of the DDR through J-link. I attached also these settings in the first post.

Best Regards,

Mohamed

0 Kudos
Reply

1,863 Views
igorpadykov
NXP Employee
NXP Employee

is that uboot working fine when loaded in usual way, not with jtag.

Probably it was wrongly built/configured.

First, suggest to check if correct uart port is configured for building uboot.imx.bin

mx6sabresd.h\configs\include - uboot-imx - i.MX U-Boot 

#define CONFIG_MXC_UART_BASE    UART1_BASE
#define CONSOLE_DEV        "ttymxc0"

Best regards
igor

0 Kudos
Reply