ECSPI1 pinout configuration on expansion connector J1003 ( imx8mm )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ECSPI1 pinout configuration on expansion connector J1003 ( imx8mm )

1,956 次查看
Chayma
Contributor III

Hello all,

I am using imx8mm and I am new with the fsl products.

I want to activate ecspi1 and use it. So, I should configure the ecspi1 pinout to link it with the connector J1003.

I searched on the forum but I couldn't find something helpful about ecspi1.

Could someone help me ?

Best regards,

标签 (1)
0 项奖励
回复
3 回复数

1,890 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chayma

one can look at overview of spi usage on i.MX8M processors

Accessing SPI Devices in Linux 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,890 次查看
Chayma
Contributor III

Hello, 

Thank you for your response . But I am using iMX8M mini board and the ecspi1 pinout are not configured in the connector j1003 so my question was how can I configure the expasion connector J1003 pins to ecspi1 pinout. 

Best regards,  

0 项奖励
回复

1,890 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复