New imx6ul-board mfgtools-downloading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New imx6ul-board mfgtools-downloading

3,923 次查看
wangqz2010
Contributor I

Dear sirs

I have a problem in downloading the programs to a new imx6ul-board using mfgtools, please see the attached file.

How can i deal with the problem, thanks a lot!

BR

标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

3,670 次查看
shivanipatel
Senior Contributor II

Hi, qizhi wang

Please refer below link which may help you.

https://community.nxp.com/thread/454298

Regards,

Shivani

0 项奖励
回复

3,670 次查看
wangqz2010
Contributor I

hi,Shivani

Thanks for your reply.

yes, I am trying to flash images in nandflash. I did it according the third-party's Board programs, please see the attached files, could you show me where the problem is? Thank you.

BEST REGARDS

WANG QIZHI

0 项奖励
回复

3,670 次查看
shivanipatel
Senior Contributor II

Hi, wangqz2010@126.com

I can not see any attached files here. Have you attached some other files or the one you have attached in the main question?

Regards,

Shivani

0 项奖励
回复

3,670 次查看
wangqz2010
Contributor I

Hi, Shivani

Could you tell what's the problem about the following messages? Thanks.

REGARDS

WQZ

U-Boot 2015.04-g5d63276bfe-dirty (Jan 10 2017 - 15:40:43)

CPU: Freescale i.MX6UL rev1.2 at 396 MHz

CPU: Temperature 47 C

Reset cause: POR

Board: MX6UL 14x14 EVK

I2C: ready

DRAM: 256 MiB

MMC: FSL_SDHC: 0, FSL_SDHC: 1

MMC: no card present

MMC init failed

Using default environment

Display: TFT43AB (480x272)

Video: 480x272x24

In: serial

Out: serial

Err: serial

MMC: no card present

Net: FEC1

Error: FEC1 address not set.

Boot from USB for mfgtools

Use default environment for mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz $ $ $;

Hit any key to stop autoboot: 0

Kernel image @ 0x80800000

    1. Loading init Ramdisk from Legacy Image at 83800000 ...

Image Name: fsl-image-mfgtool-initramfs-imx_

Image Type: ARM Linux RAMDisk Image (gzip compressed)

Data Size: 7485694 Bytes = 7.1 MiB

Load Address: 00000000

Entry Point: 00000000

Verifying Checksum ... OK

    1. Flattened Device Tree blob at 83000000

Booting using the fdt blob at 0x83000000

Using Device Tree in place at 83000000, end 8300c60a

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 3.14.38+ (root@develop) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #4 SMP PREEMPT Mon Jan 9 09:53:31 CST 2017

CPU: ARMv7 Processor revision 5 (ARMv7), cr=10c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board

cma: CMA: reserved 64 MiB at 8c000000

Memory policy: Data cache writealloc

PERCPU: Embedded 8 pages/cpu @8bdbf000 s8320 r8192 d16256 u32768

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024

Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc cma=64m g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused

PID hash table entries: 1024 (order: 0, 4096 bytes)

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 176672K/262144K available (6712K kernel code, 347K rwdata, 2216K rodata, 360K init, 418K bss, 85472K reserved, 0K highmem)

Virtual kernel memory layout:

vector : 0xffff0000 - 0xffff1000 ( 4 kB)

fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

vmalloc : 0x90800000 - 0xff000000 (1768 MB)

lowmem : 0x80000000 - 0x90000000 ( 256 MB)

pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

.text : 0x80008000 - 0x808c02e8 (8929 kB)

.init : 0x808c1000 - 0x8091b080 ( 361 kB)

.data : 0x8091c000 - 0x80972fa0 ( 348 kB)

.bss : 0x80972fac - 0x809dba50 ( 419 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1

NR_IRQS:16 nr_irqs:16 16

Switching to timer-based delay loop

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns

clocksource_of_init: no matching clocksources found

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

/cpus/cpu@0 missing clock-frequency property

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x8065f4f8 - 0x8065f568

Brought up 1 CPUs

SMP: Total of 1 processors activated (6.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap registered

vdd3p0: 2625 <--> 3400 mV at 3000 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e4000.iomuxc-gpr: regmap registered

syscon 21ac000.romcp: regmap registered

syscon 21bc000.ocotp-ctrl: regmap registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/csi1grp

imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/i2c2grp

imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

20dc000.gpc supply pu not found, using dummy regulator

bio: create slab <bio-0> at 0

mxs-dma 1804000.dma-apbh: initialized

can-3v3: 3300 mV

VSD_3V3: 3300 mV

usb_otg1_vbus: 5000 mV

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource mxc_timer1

cfg80211: Calling CRDA to update world regulatory domain

NET: Registered protocol family 2

TCP established hash table entries: 2048 (order: 1, 8192 bytes)

TCP bind hash table entries: 2048 (order: 2, 16384 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP: reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 7304K (83801000 - 83f23000)

imx rpmsg driver is registered.

Bus freq driver module loaded

futex hash table entries: 256 (order: 2, 16384 bytes)

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 487

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: Driver registered.

backlight.8 supply power not found, using dummy regulator

MIPI DSI driver module loaded

21c8000.lcdif supply lcd not found, using dummy regulator

mxsfb 21c8000.lcdif: failed to find mxc display driver

Console: switching to colour frame buffer device 100x30

mxsfb 21c8000.lcdif: initialized

imx-sdma 20ec000.sdma: no event needs to be remapped

imx-sdma 20ec000.sdma: loaded firmware 3.1

imx-sdma 20ec000.sdma: initialized

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX

console enabled

21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX

21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX

21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62, base_baud = 5000000) is a IMX

serial: Freescale lpuart driver

imx sema4 driver is registered.

Initialized drm 1.1.0 20060810

Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

nand: Could not find valid ONFI parameter page; aborting

nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3

nand: Micron NAND 1GiB 3,3V 8-bit

nand: 1024MiB, SLC, page size: 4096, OOB size: 128

Scanning device for bad blocks

gpmi-nand 1806000.gpmi-nand: DMA timeout, last DMA :1

gpmi-nand 1806000.gpmi-nand: Show GPMI registers :

gpmi-nand 1806000.gpmi-nand: offset 0x000 : 0x21800080

gpmi-nand 1806000.gpmi-nand: offset 0x010 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x020 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x030 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x040 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x050 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x060 : 0x0104000c

gpmi-nand 1806000.gpmi-nand: offset 0x070 : 0x00010203

gpmi-nand 1806000.gpmi-nand: offset 0x080 : 0x05000000

gpmi-nand 1806000.gpmi-nand: offset 0x090 : 0x23023336

gpmi-nand 1806000.gpmi-nand: offset 0x0a0 : 0xffffffff

gpmi-nand 1806000.gpmi-nand: offset 0x0b0 : 0xff000005

gpmi-nand 1806000.gpmi-nand: offset 0x0c0 : 0x00000100

gpmi-nand 1806000.gpmi-nand: offset 0x0d0 : 0x05020000

gpmi-nand 1806000.gpmi-nand: Show BCH registers :

gpmi-nand 1806000.gpmi-nand: offset 0x000 : 0x00000100

gpmi-nand 1806000.gpmi-nand: offset 0x010 : 0x00000010

gpmi-nand 1806000.gpmi-nand: offset 0x020 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x030 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x040 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x050 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x060 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x070 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x080 : 0x070a2080

gpmi-nand 1806000.gpmi-nand: offset 0x090 : 0x10802080

gpmi-nand 1806000.gpmi-nand: offset 0x0a0 : 0x070a4080

gpmi-nand 1806000.gpmi-nand: offset 0x0b0 : 0x10da4080

gpmi-nand 1806000.gpmi-nand: offset 0x0c0 : 0x070a4080

gpmi-nand 1806000.gpmi-nand: offset 0x0d0 : 0x10da4080

gpmi-nand 1806000.gpmi-nand: offset 0x0e0 : 0x070a4080

gpmi-nand 1806000.gpmi-nand: offset 0x0f0 : 0x10da4080

gpmi-nand 1806000.gpmi-nand: offset 0x100 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x110 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x120 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x130 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x140 : 0x00000000

gpmi-nand 1806000.gpmi-nand: offset 0x150 : 0x20484342

gpmi-nand 1806000.gpmi-nand: offset 0x160 : 0x01000000

gpmi-nand 1806000.gpmi-nand: offset 0x170 : 0x00000000

gpmi-nand 1806000.gpmi-nand: BCH Geometry :

GF length : 13

ECC Strength : 8

Page Size in Bytes : 4224

Metadata Size in Bytes : 10

ECC Chunk Size in Bytes: 512

ECC Chunk Count : 8

Payload Size in Bytes : 4096

Auxiliary Size in Bytes: 20

Auxiliary Status Offset: 12

Block Mark Byte Offset : 3995

Block Mark Bit Offset : 0

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

.

.

.

.

.

.

.

.

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

8 ofpart partitions found on MTD device gpmi-nand

Creating 8 MTD partitions on "gpmi-nand":

0x000000000000-0x000000800000 : "boot"

0x000000800000-0x000000a00000 : "logo"

0x000000a00000-0x000000b00000 : "ENV"

0x000000b00000-0x000000e00000 : "DTB"

0x000000e00000-0x000001600000 : "kernel"

0x000001600000-0x000001700000 : "DTBbak"

0x000001700000-0x000001f00000 : "kernelbak"

0x000001f00000-0x000040000000 : "rootfs"

gpmi-nand 1806000.gpmi-nand: driver registered.

20b4000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

fec 20b4000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 20b4000.ethernet (unregistered net_device): Using random MAC address: 86:29:9b:2c:72:c8

libphy: fec_enet_mii_bus: probed

fec 20b4000.ethernet eth0: registered PHC device 0

2188000.ethernet supply phy not found, using dummy regulator

pps pps1: new PPS source ptp1

fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 2188000.ethernet (unregistered net_device): Using random MAC address: 8e:1d:09:65:ab:39

fec 2188000.ethernet eth1: registered PHC device 1

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

2184800.usbmisc supply vbus-wakeup not found, using dummy regulator

2184200.usb supply vbus not found, using dummy regulator

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

rtc-rx8010 0-0032: Unable to write register #23

i2c i2c-0: probing for rx8010 failed

rtc-rx8010: probe of 0-0032 failed with error -5

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR RC5 (streamzap) protocol handler initialized

IR SANYO protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

pxp-v4l2 pxp_v4l2.9: initialized

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: no vqmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc using ADMA

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

TCP: cubic registered

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

Key type dns_resolver registered

cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)

Registering SWP/SWPB emulation handler

usb_otg1_vbus: disabling

VSD_3V3: disabling

can-3v3: disabling

regulator-dummy: disabling

imx mcc test is registered.

Number of LUNs=8

Mass Storage Function, version: 2009/09/11

LUN: removable file: (no medium)

Number of LUNs=1

LUN: removable file: (no medium)

Number of LUNs=1

g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11

g_mass_storage gadget: g_mass_storage ready

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)

clk: Not disabling unused clocks

ALSA device list:

No soundcards found.

Freeing unused kernel memory: 360K (808c1000 - 8091b000)

Starting UTP

uuc 0.5

UTP: Waiting for device to appear

UTP: file/device node /dev/utp already exists

cpu_id is 0

g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage

UTP: received command '$ cat /proc/mtd '

UTP: executing "cat /proc/mtd "

dev: size erasesize name

mtd0: 00800000 00040000 "boot"

mtd1: 00200000 00040000 "logo"

mtd2: 00100000 00040000 "ENV"

mtd3: 00300000 00040000 "DTB"

mtd4: 00800000 00040000 "kernel"

mtd5: 00100000 00040000 "DTBbak"

mtd6: 00800000 00040000 "kernelbak"

mtd7: 3e100000 00040000 "rootfs"

UTP: sending Success to kernel for command $ cat /proc/mtd .

utp_poll: pass returned.

UTP: received command '$ flash_eraseall /dev/mtd0'

UTP: executing "flash_eraseall /dev/mtd0"

flash_eraseall has been replaced by `flash_erase 0 0`; please use it

Erasing 256 Kibyte @ 0 -- 0 % cgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

omplete libmtd: error!: MEMERASE64 ioctlgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

failed for eraseblock 0 (mtd0)

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error 5 (Input/output errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

or)

flash_erase: error!: /dev/mtgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

d0: MTD Erase failure

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error 5 (Input/output error)

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

Erasing 256 Kibyte @ 40000 -- 3gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

% complete libmtd: error!: MEMERgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

ASE64 ioctl failed for eraseblockgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

1 (mtd0)

error 5 (Inputgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

/output error)

flash_erase: errogpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error 5 (Input/outpgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

ut error)

Erasing 256 Kibyte @ gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

80000 -- 6 % complete libmtd: ergpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

ror!: MEMERASE64 ioctl failed forgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

eraseblock 2 (mtd0)

errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

or 5 (Input/output error)

flash_gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

erase: error!: /dev/mtd0: MTD Eragpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

se failure

error 5 (Input/output error)

Erasing 256 Kibyte @ c0000 -- 9 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 3 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 100000 -- 12 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 4 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 140000 -- 15 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 5 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 180000 -- 18 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 6 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 1c0000 -- 21 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 7 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 200000 -- 25 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 8 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 240000 -- 28 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 9 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 280000 -- 31 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 10 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 2c0000 -- 34 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 11 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 300000 -- 37 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 12 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 340000 -- 40 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 13 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 380000 -- 43 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 14 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 3c0000 -- 46 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 15 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 400000 -- 50 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 16 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 440000 -- 53 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 17 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 480000 -- 56 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 18 (mtd0)

error 5 (Input/output error)

flash_erase: errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

or!: /dev/mtd0: MTD Erase failuregpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error 5 (Input/outgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

put error)

Erasing 256 Kibyte @gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

4c0000 -- 59 % complete libmtd: gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error!: MEMERASE64 ioctl failed fgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

or eraseblock 19 (mtd0)

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

error 5 (Input/output error)

flagpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

sh_erase: error!: /dev/mtd0: MTD gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

Erase failure

errorgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

5 (Input/output error)

Erasinggpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

256 Kibyte @ 500000 -- 62 % compgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

lete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 20 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 540000 -- 65 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 21 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 580000 -- 68 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 22 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 5c0000 -- 71 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 23 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 600000 -- 75 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 24 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 640000 -- 78 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 25 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 680000 -- 81 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 26 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtutp_poll: pass returned.

d0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 6c0000 -- 84 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 27 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 700000 -- 87 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 28 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 740000 -- 90 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 29 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 780000 -- 93 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 30 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 7c0000 -- 96 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 31 (mtd0)

error 5 (Input/output error)

flash_erase: error!: /dev/mtd0: MTD Erase failure

error 5 (Input/output error)

Erasing 256 Kibyte @ 7c0000 -- 100 % complete

UTP: sending Success to kernel for command $ flash_eraseall /dev/mtd0.

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ ls $FILE'

UTP: executing "ls $FILE"

/tmp/file.utp

UTP: sending Success to kernel for command $ ls $FILE.

utp_poll: pass returned.

UTP: received command '$ kobs-ng init -x $FILE '

UTP: executing "kobs-ng init -x $FILE "

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

mtd: device 0 fails MEMERASE (0x0gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

- 0x40000)

mtd: Failed to erasegpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

block @0x0

mtd: device 0 fails gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

MEMERASE (0x40000 - 0x40000)

mtdgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

mtd: device 0 fails MEMERASE (0xgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

80000 - 0x40000)

mtd: Failed to gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

erase block @0x80000

mtd: devicegpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

0 fails MEMERASE (0xc0000 - 0x40gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

000)

mtd: Failed to erase block gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

@0xc0000

mtd: device 0 fails MEMgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

ERASE (0x100000 - 0x40000)

mtd: gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

Failed to erase block @0x100000

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

mtd: device 0 fails MEMERASE (0x1gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

40000 - 0x40000)

mtd: Failed to gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

erase block @0x140000

mtd: devicgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

e 0 fails MEMERASE (0x180000 - 0xgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

40000)

mtd: Failed to erase blocgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

k @0x180000

mtd: device 0 fails gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

MEMERASE (0x1c0000 - 0x40000)

mtgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

d: Failed to erase block @0x1c0000

mtd: device 0 fails MEMERASE (0x200000 - 0x40000)

mtd: Failed to erase block@0x200000

mtd: device 0 fails MEMERASE (0x240000 - 0x40000)

mtd: Failed to erase block@0x240000

mtd: device 0 fails MEMERASE (0x280000 - 0x40000)

mtd: Failed to erase block@0x280000

mtd: device 0 fails MEMERASE (0x2c0000 - 0x40000)

mtd: Failed to erase block@0x2c0000

mtd: device 0 fails MEMERASE (0x300000 - 0x40000)

mtd: Failed to erase block@0x300000

mtd: device 0 fails MEMERASE (0x340000 - 0x40000)

mtd: Failed to erase block@0x340000

mtd: device 0 fails MEMERASE (0x380000 - 0x40utp_poll: exit with status 1280

000)

mtd: Failed to erase block@0x380000

mtd: device 0 fails MEMERASE (0x3c0000 - 0x40000)

mtd: Failed to erase block@0x3c0000

mtd: device 0 fails MEMERASE (0x400000 - 0x40000)

mtd: Failed to erase block@0x400000

mtd: device 0 fails MEMERASE (0x440000 - 0x40000)

mtd: Failed to erase block@0x440000

mtd: device 0 fails MEMERASE (0x480000 - 0x40000)

mtd: Failed to erase block@0x480000

mtd: device 0 fails MEMERASE (0x4c0000 - 0x40000)

mtd: Failed to erase block@0x4c0000

mtd: mtd_write_page failed

Failed to write safe page

mtd: Failed to write BS#0

FAILED to commit structures

UTP: sending Non-success to kernel for command $ kobs-ng init -x $FILE .

random: nonblocking pool is initialized

gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22

0 项奖励
回复

3,669 次查看
wangqz2010
Contributor I

Hi, Shivani

The mfgtool-files is too big to be sent, which i used is V2 version;  Please find the attached schematic files, is it the hardware problem or the software problem. Because I am a newer in embedded Linux, I don't know how to modify software. THANKS

Regards,

Wang QiZHi

0 项奖励
回复

3,669 次查看
shivanipatel
Senior Contributor II

Hi, wangqz2010@126.com

Have you referred the link I have shared previously?

IMX6UL-EVK Programming NAND via L4.1.15_2.0.0-ga_mfg-tools 

Please go through the above given link. You need to add support for NAND in your software using "imx_v7_mfg_defconfig". In the above link it is given that how you can generate the NAND supported zImage and DTB. These files you need to copy in the mfgtool at "mfgtools/Profiles/Linux/OS Firmware/files/" path. After that you can flash with the .vbs script.

Regards,

Shivani

0 项奖励
回复

3,669 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? If you are using the newest BSP, you can refer to https://community.nxp.com/thread/517143 

0 项奖励
回复