Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

跳至解决方案
1,756 次查看
RobbieJiang
Contributor IV

Hi,

Currently the 'tvsrc' element works with my CSI camera on MX6Q/Linux platform.

However, we would like to make some changes to 'tvsrc', e.g, to add some new attributes,

or to support more input resolutions.

So the source code of 'tvsrc' is needed.

But I have only the binary code of libmfw_gst_tvsrc.so,

where can I get the source code?

Regards,

Jie

标签 (3)
1 解答
1,503 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

在原帖中查看解决方案

4 回复数
1,503 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

had you looked in gst-fsl-plugins L3.0.35_4.1.0_MM_CODECS

Middleware-Codecs and other Algorithms (11)

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

0 项奖励
回复
1,503 次查看
RobbieJiang
Contributor IV

Hi igor,

In the codecs packaged you mentioned,

there is no source code for tvsrc.

Is it a third party software?

Why is fsl's 'mfw_v4lsrc'  not used and replaced by tvsrc?

Regards,

Robbie

0 项奖励
回复
1,504 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

1,503 次查看
RobbieJiang
Contributor IV

Hi igor,

Thanks for your information.

I tried to download  L3.0.35_4.1.0_MM_CODECS,

but actually it is included in L3.0.101_4.1.1_MM_CODECS.

Anyway,  thanks a lot!

Regards,

Jie

0 项奖励
回复