Hi,
Currently the 'tvsrc' element works with my CSI camera on MX6Q/Linux platform.
However, we would like to make some changes to 'tvsrc', e.g, to add some new attributes,
or to support more input resolutions.
So the source code of 'tvsrc' is needed.
But I have only the binary code of libmfw_gst_tvsrc.so,
where can I get the source code?
Regards,
Jie
解決済! 解決策の投稿を見る。
Hi Robbie
had you looked in gst-fsl-plugins L3.0.35_4.1.0_MM_CODECS
Middleware-Codecs and other Algorithms (11)
i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
Best regards
igor
Hi igor,
In the codecs packaged you mentioned,
there is no source code for tvsrc.
Is it a third party software?
Why is fsl's 'mfw_v4lsrc' not used and replaced by tvsrc?
Regards,
Robbie
Hi Robbie
in gst-fsl-plugins-3.0.11.tar.gz I found
~igor
Hi igor,
Thanks for your information.
I tried to download L3.0.35_4.1.0_MM_CODECS,
but actually it is included in L3.0.101_4.1.1_MM_CODECS.
Anyway, thanks a lot!
Regards,
Jie