Need second gpio pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need second gpio pin

跳至解决方案
2,226 次查看
jimpanse
Contributor II

Hey folks,

I'm already toggling the USER led on my i.MX53 QSB via the GPIO7 register. That works pretty fine.

Now I need a second GPIO pin that i can control via software and that is (easily) accessible from

outside.

Can U help me? Thanks in advance!

标签 (1)
标记 (3)
1 解答
2,107 次查看
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

在原帖中查看解决方案

2 回复数
2,108 次查看
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

2,107 次查看
jimpanse
Contributor II

Thank you very much! Perfect answer!

0 项奖励
回复