Need SDK or code to reset the RTC for imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need SDK or code to reset the RTC for imx6q

2,267件の閲覧回数
Aravinthkumar
Contributor III

Hi Team,

I want to know how to reset the RTC from nxp SDK. We have some existing setup using to reset the RTC and other hardware testing. I'm attaching the tera tera response here. Can you please share SDK related to that and how to flash to the device.

RTC_reset_1.jpg

 

Regards,

Aravinth 

ラベル(6)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,195件の閲覧回数
Aravinthkumar
Contributor III

Hi Team,

As I checked the issue, In the RTC month (07h Century_months) register value become 0. As per datasheet it never goes to 0.

Can you please provide the reason for this issue.

 

Regards,

Aravinth

 

0 件の賞賛
返信

2,166件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Aravinthkumar 

I hope you are doing well
 
RTC month (07h Century_months) register value become 0
=> Kindly mention which register you are trying to read. Please mention how you are reading that register.
 
 As per datasheet it never goes to 0.
=> Please add more details, i.e., register name and where it is mentioned in the datasheet.
 
Thanks & Regards
Sanket Parekh

0 件の賞賛
返信

2,239件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
For the SDK for the IMX6 series, Please refer to the below thread.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信