Need SDK or code to reset the RTC for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need SDK or code to reset the RTC for imx6q

2,232 Views
Aravinthkumar
Contributor III

Hi Team,

I want to know how to reset the RTC from nxp SDK. We have some existing setup using to reset the RTC and other hardware testing. I'm attaching the tera tera response here. Can you please share SDK related to that and how to flash to the device.

RTC_reset_1.jpg

 

Regards,

Aravinth 

Tags (4)
0 Kudos
Reply
3 Replies

2,160 Views
Aravinthkumar
Contributor III

Hi Team,

As I checked the issue, In the RTC month (07h Century_months) register value become 0. As per datasheet it never goes to 0.

Can you please provide the reason for this issue.

 

Regards,

Aravinth

 

0 Kudos
Reply

2,131 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Aravinthkumar 

I hope you are doing well
 
RTC month (07h Century_months) register value become 0
=> Kindly mention which register you are trying to read. Please mention how you are reading that register.
 
 As per datasheet it never goes to 0.
=> Please add more details, i.e., register name and where it is mentioned in the datasheet.
 
Thanks & Regards
Sanket Parekh

0 Kudos
Reply

2,204 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
For the SDK for the IMX6 series, Please refer to the below thread.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply