Need Code Signing Tool V2.3.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need Code Signing Tool V2.3.1

ソリューションへジャンプ
1,886件の閲覧回数
JimBaxter
Contributor III

Hi, we need access to an older NXP Code Signing Tool V 2.3.1 as the V2.3.2 does not work with the project source I am working with, is there a way to download  an archived version of the tool?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,764件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,765件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信