Need Code Signing Tool V2.3.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Code Signing Tool V2.3.1

Jump to solution
1,973 Views
JimBaxter
Contributor III

Hi, we need access to an older NXP Code Signing Tool V 2.3.1 as the V2.3.2 does not work with the project source I am working with, is there a way to download  an archived version of the tool?

Labels (3)
0 Kudos
Reply
1 Solution
1,851 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,852 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply