NXP i.MX8M Mini System kernel panic in Yocto 2.5.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP i.MX8M Mini System kernel panic in Yocto 2.5.

1,067件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP 

Our customer use the i.MX8M Mini solution. (Yocto 2.5)

He try modify and add rs-485 application.

** drivers/tty/serial/imx.c **     

-#define RXTL_UART 16 /* For uart */
+#define RXTL_UART 4 /* For uart */

He run the application, then debug message show "kernel panic".

Please check the modify patch. (0001_tsl_kernel_modify.patch) and System Crash_info.txt 

Our customer try modify the RXTL_UART  4 (in driver/tty/serial/imx.c)

Do you have any advice about fixed the kernel panic issue?

 

 

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,025件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

By the error it is a failed read access, more information about this can be found in the D3.5 ARMv8 Architecture Reference Manual.

It may be useful to look into the following commit:

https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&id=677fe555cbfb188af58cce10...

Also, would it be possible to try with a more recent kernel release?

Best regards,
Aldo.

0 件の賞賛
返信