NXP i.MX8M Mini System kernel panic in Yocto 2.5.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP i.MX8M Mini System kernel panic in Yocto 2.5.

1,625 Views
charleshuang
Senior Contributor II

Hi NXP 

Our customer use the i.MX8M Mini solution. (Yocto 2.5)

He try modify and add rs-485 application.

** drivers/tty/serial/imx.c **     

-#define RXTL_UART 16 /* For uart */
+#define RXTL_UART 4 /* For uart */

He run the application, then debug message show "kernel panic".

Please check the modify patch. (0001_tsl_kernel_modify.patch) and System Crash_info.txt 

Our customer try modify the RXTL_UART  4 (in driver/tty/serial/imx.c)

Do you have any advice about fixed the kernel panic issue?

 

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,583 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

By the error it is a failed read access, more information about this can be found in the D3.5 ARMv8 Architecture Reference Manual.

It may be useful to look into the following commit:

https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&id=677fe555cbfb188af58cce10...

Also, would it be possible to try with a more recent kernel release?

Best regards,
Aldo.

0 Kudos
Reply