NXP i.MX6ULL EVK and Linux Kernel CONFIG_SMP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP i.MX6ULL EVK and Linux Kernel CONFIG_SMP

1,169 次查看
daweichen
Contributor III

The default kernel configuration file for i.MX6ULL EVK has the CONFIG_SMP set.

I was wondering if the CONFIG_SMP should be set for uniprocessor systems like i.MX6ULL.

If so, what would be a use case or a reason for enabling CONFIG_SMP?

My understanding is that CONFIG_SMP should be unset for uniprocessor systems for efficiency.

Thank you so much,

Dawei

标签 (3)
0 项奖励
回复
1 回复

1,081 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

you are right, for processor with one core linux CONFIG_SMP is not needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复