NXP MCIMX8M Mini Yocto Building system Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MCIMX8M Mini Yocto Building system Issue

Jump to solution
6,811 Views
DanielDuJijun
Contributor III

Dear NXP Supporting Team.

would you please kindly help to check the following error and warning.

Could you help to give some advice?

thanks

Linux Branch : L5.10.72

 

crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72$ source setup-environment build-wayland

Welcome to Freescale Community BSP

The Yocto Project has extensive documentation about OE including a
reference manual which can be found at:
    http://yoctoproject.org/documentation

For more information about OpenEmbedded see their website:
    http://www.openembedded.org/

You can now run 'bitbake <target>'

Common targets are:
    core-image-minimal
    meta-toolchain
    meta-toolchain-sdk
    adt-installer
    meta-ide-support

Your configuration files at build-wayland have not been touched.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$ bitbake -k imx-image-full --runall=fetch

 

Error as following :

 

Initialising tasks: 100% |################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 0 Local 0 Network 0 Missed 0 Current 0 (0% match, 0% complete)
NOTE: No setscene tasks
NOTE: Executing Tasks
WARNING: onnxruntime-1.8.2-r0 do_fetch: Failed to fetch URL gitsm://github.com/nxp-imx/onnxruntime-imx.git;protocol=https;branch=lf-5.10.72_2.2.0, attempting MIRRORS if available
ERROR: onnxruntime-1.8.2-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export PATH="/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/bin/python3-native:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/poky/scripts:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot/usr/bin/crossscripts:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/sbin:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/bin:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/sbin:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/bin:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/poky/bitbake/bin:/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/hosttools"; export HOME="/home/crp"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror https://github.com/nxp-imx/onnxruntime-imx.git /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/downloads//git2/github.com.nxp-imx.onnxruntime-imx.git --progress failed with exit code 128, no output
ERROR: onnxruntime-1.8.2-r0 do_fetch: Fetcher failure for URL: 'gitsm://github.com/nxp-imx/onnxruntime-imx.git;protocol=https;branch=lf-5.10.72_2.2.0'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/temp/log.do_fetch.19344
ERROR: Task (/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.8.2.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 661 tasks of which 660 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.8.2.bb:do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$

Labels (2)
0 Kudos
Reply
1 Solution
6,554 Views
DanielDuJijun
Contributor III

Hi Joan Xie.

thanks a lot for your support.

i have checked the link

"https://stackoverflow.com/questions/72424674/is-there-a-solution-for-the-odd-error-of-bitbake"

But i have no idea that it can fix my problem.

please check and advice.

thanks.

View solution in original post

0 Kudos
Reply
10 Replies
6,600 Views
DanielDuJijun
Contributor III

Dear NXP Support Team.

please check the log as following.

I can git clone from git clone https://github.com/microsoft/onnxruntime-tvm.git

So I do not think this should be network issue.

would you help to check and give some advice?

Thanks.

 

               crp@crp-ubuntu:~$ mkdir temp_onnxruntime

crp@crp-ubuntu:~$ cd temp_onnxruntime/

crp@crp-ubuntu:~/temp_onnxruntime$ git clone https://github.com/microsoft/onnxruntime-tvm.git

Cloning into 'onnxruntime-tvm'...

remote: Enumerating objects: 47548, done.

remote: Counting objects: 100% (130/130), done.

remote: Compressing objects: 100% (47/47), done.

remote: Total 47548 (delta 93), reused 83 (delta 83), pack-reused 47418

Receiving objects: 100% (47548/47548), 16.85 MiB | 1.74 MiB/s, done.

Resolving deltas: 100% (32014/32014), done.

 

 

            2,718 items, totalling 35.8 MB of temp_onnxruntime/

crp@crp-ubuntu:~$ cd temp_onnxruntime/
crp@crp-ubuntu:~/temp_onnxruntime$ ls
onnxruntime-tvm
crp@crp-ubuntu:~/temp_onnxruntime$ cd onnxruntime-tvm/
crp@crp-ubuntu:~/temp_onnxruntime/onnxruntime-tvm$ ls
3rdparty         docker       LICENSE   README.md    tutorials
apps             docs         Makefile  rust         version.py
cmake            golang       NEWS.md   SECURITY.md  vta
CMakeLists.txt   include      nnvm      src          web
conda            Jenkinsfile  NOTICE    tests
CONTRIBUTORS.md  jvm          python    topi
crp@crp-ubuntu:~/temp_onnxruntime/onnxruntime-tvm$

0 Kudos
Reply
6,736 Views
DanielDuJijun
Contributor III

Dear NXP Support Team;

please check the update as following :

crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$ bitbake -c cleansstate connxruntime
Loading cache: 100% |#####################################################################################################################| Time: 0:00:00
Loaded 4951 entries from dependency cache.
ERROR: Nothing PROVIDES 'connxruntime'. Close matches:
go-runtime
onnxruntime
onnxruntime-native

Summary: There was 1 ERROR message shown, returning a non-zero exit code.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$

 

Initialising tasks: 100% |################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 761 Local 0 Network 0 Missed 761 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
ERROR: armnn-onnx-protobuf-1.6.0-r0 do_unpack: Unpack failure for URL: 'git://github.com/onnx/onnx.git;branch=rel-1.6.0'. No up to date source found: clone directory not available or not up to date: /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/downloads//git2/github.com.onnx.onnx.git; shallow clone not enabled
ERROR: Logfile of failure stored in: /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/armnn-onnx-protobuf/1.6.0-r0/temp/log.do_unpack.22933
ERROR: Task (/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx-protobuf_1.6.0.bb:do_unpack) failed with exit code '1'
NOTE: Tasks Summary: Attempted 473 tasks of which 165 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx-protobuf_1.6.0.bb:do_unpack
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$

0 Kudos
Reply
6,620 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems you type the wrong command, should be onnxruntime, not connxruntime

0 Kudos
Reply
6,611 Views
DanielDuJijun
Contributor III

Yes,You are right that i type the wrong words

but i had test it right now.There are some error about it .

please help to check the log as folloing :

 

 

crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$ bitbake -c cleansstate onnxruntime
Loading cache: 100% |#####################################################################################################################| Time: 0:00:00
Loaded 4951 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.50.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.10-hardknott"
TUNE_FEATURES = "aarch64 armv8a crc cortexa53 crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:269265c00091fa65f93de6cad32bf24f1e7f72a3"
meta-oe
meta-multimedia
meta-python = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-freescale = "HEAD:469d6c958c76ea235b3d3c1527e797ce3a7392e3"
meta-freescale-3rdparty = "HEAD:f8150f3b37cb83cba1f9e2378e57bb63e02d4610"
meta-freescale-distro = "HEAD:e6daa26ba1f748326546063d63a085ae671827d9"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:d176aee3567cdccb5a7fb7c7e70a7cb3bee51bc0"
meta-nxp-demo-experience = "HEAD:f540304fda6242be240792095ec4a67bfbb9425f"
meta-chromium = "HEAD:8be1d3a0ba0cf32e61144900597207af5698c10d"
meta-clang = "HEAD:b0d805060791006d651efd3d7ae3dd5add8f70fe"
meta-gnome
meta-networking
meta-filesystems = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-qt5 = "HEAD:43f8f539d40070a70fe89136db89bf5bb1dfe7ed"
meta-python2 = "HEAD:8db9e4f6ceae33d7a4f55453d31e69f9858af4eb"
meta-virtualization = "HEAD:7f719ef40896b6c78893add8485fda995b00d51d"

Initialising tasks: 100% |################################################################################################################| Time: 0:00:00
Sstate summary: Wanted 0 Local 0 Network 0 Missed 0 Current 0 (0% match, 0% complete)
NOTE: No setscene tasks
NOTE: Executing Tasks
NOTE: Tasks Summary: Attempted 2 tasks of which 0 didn't need to be rerun and all succeeded.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$ bitbake onnxruntime
Loading cache: 100% |#####################################################################################################################| Time: 0:00:00
Loaded 4951 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.50.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.10-hardknott"
TUNE_FEATURES = "aarch64 armv8a crc cortexa53 crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:269265c00091fa65f93de6cad32bf24f1e7f72a3"
meta-oe
meta-multimedia
meta-python = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-freescale = "HEAD:469d6c958c76ea235b3d3c1527e797ce3a7392e3"
meta-freescale-3rdparty = "HEAD:f8150f3b37cb83cba1f9e2378e57bb63e02d4610"
meta-freescale-distro = "HEAD:e6daa26ba1f748326546063d63a085ae671827d9"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:d176aee3567cdccb5a7fb7c7e70a7cb3bee51bc0"
meta-nxp-demo-experience = "HEAD:f540304fda6242be240792095ec4a67bfbb9425f"
meta-chromium = "HEAD:8be1d3a0ba0cf32e61144900597207af5698c10d"
meta-clang = "HEAD:b0d805060791006d651efd3d7ae3dd5add8f70fe"
meta-gnome
meta-networking
meta-filesystems = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-qt5 = "HEAD:43f8f539d40070a70fe89136db89bf5bb1dfe7ed"
meta-python2 = "HEAD:8db9e4f6ceae33d7a4f55453d31e69f9858af4eb"
meta-virtualization = "HEAD:7f719ef40896b6c78893add8485fda995b00d51d"

Initialising tasks: 100% |################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 686 Local 0 Network 0 Missed 686 Current 75 (0% match, 9% complete)
NOTE: Executing Tasks
ERROR: armnn-onnx-protobuf-1.6.0-r0 do_unpack: Unpack failure for URL: 'git://github.com/onnx/onnx.git;branch=rel-1.6.0'. No up to date source found: clone directory not available or not up to date: /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/downloads//git2/github.com.onnx.onnx.git; shallow clone not enabled
ERROR: Logfile of failure stored in: /home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland/tmp/work/cortexa53-crypto-poky-linux/armnn-onnx-protobuf/1.6.0-r0/temp/log.do_unpack.6385
ERROR: Task (/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx-protobuf_1.6.0.bb:do_unpack) failed with exit code '1'
NOTE: Tasks Summary: Attempted 489 tasks of which 480 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/crp/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx-protobuf_1.6.0.bb:do_unpack
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
crp@crp-ubuntu:~/crp-nxp-imx8mm-yocto-linux-bsp-l5.10.72/build-wayland$

0 Kudos
Reply
6,562 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
6,555 Views
DanielDuJijun
Contributor III

Hi Joan Xie.

thanks a lot for your support.

i have checked the link

"https://stackoverflow.com/questions/72424674/is-there-a-solution-for-the-odd-error-of-bitbake"

But i have no idea that it can fix my problem.

please check and advice.

thanks.

0 Kudos
Reply
6,489 Views
joanxie
NXP TechSupport
NXP TechSupport

could you share your build steps? the source code moved from https://source.codeaurora.org/ to github.com, I'm not sure if you change repo init from https://source.codeaurora.org/ to github.com, maybe you need check your bb file, then change the source or build this bsp from begging, change the repo init from https://source.codeaurora.org/ to github.com

0 Kudos
Reply
6,569 Views
DanielDuJijun
Contributor III

Dear NXP Support Team.

please check the log as following.

I can git clone from git clone https://github.com/microsoft/onnxruntime-tvm.git

So I do not think this should be network issue.

would you help to check and give some advice?

Thanks.

 

               crp@crp-ubuntu:~$ mkdir temp_onnxruntime

crp@crp-ubuntu:~$ cd temp_onnxruntime/

crp@crp-ubuntu:~/temp_onnxruntime$ git clone https://github.com/microsoft/onnxruntime-tvm.git

Cloning into 'onnxruntime-tvm'...

remote: Enumerating objects: 47548, done.

remote: Counting objects: 100% (130/130), done.

remote: Compressing objects: 100% (47/47), done.

remote: Total 47548 (delta 93), reused 83 (delta 83), pack-reused 47418

Receiving objects: 100% (47548/47548), 16.85 MiB | 1.74 MiB/s, done.

Resolving deltas: 100% (32014/32014), done.

 

 

            2,718 items, totalling 35.8 MB of temp_onnxruntime/

crp@crp-ubuntu:~$ cd temp_onnxruntime/
crp@crp-ubuntu:~/temp_onnxruntime$ ls
onnxruntime-tvm
crp@crp-ubuntu:~/temp_onnxruntime$ cd onnxruntime-tvm/
crp@crp-ubuntu:~/temp_onnxruntime/onnxruntime-tvm$ ls
3rdparty         docker       LICENSE   README.md    tutorials
apps             docs         Makefile  rust         version.py
cmake            golang       NEWS.md   SECURITY.md  vta
CMakeLists.txt   include      nnvm      src          web
conda            Jenkinsfile  NOTICE    tests
CONTRIBUTORS.md  jvm          python    topi
crp@crp-ubuntu:~/temp_onnxruntime/onnxruntime-tvm$

0 Kudos
Reply
6,536 Views
joanxie
NXP TechSupport
NXP TechSupport

 I mean this issue "ERROR: onnxruntime-1.8.2-r0 do_fetch: Fetcher failure:" is network issue, for your second unpack issue, I send the link to you for reference, this isn't network issue

0 Kudos
Reply
6,758 Views
joanxie
NXP TechSupport
NXP TechSupport

this should be network issue, try to use command "bitbake -c cleansstate onnxruntime" to clean this package and bitbake again "bitbake onnxruntime", if still failed, pls tell me

0 Kudos
Reply