NXP IMX8M Mini Booting Fail problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP IMX8M Mini Booting Fail problem

9,812 Views
DanielDuJijun
Contributor III

Dear NXP Supporting Team;

We have some IMX8M Mini Core board booting fails problem.

The attached is the booting failed logs.

would you please kindly help to check and give some advice?

thanks.

0 Kudos
Reply
6 Replies

9,671 Views
DanielDuJijun
Contributor III

@Harvey021 

Yes.

All these boot failure for i.MX8MM but in different board and all BSP is 5.4.70.

0 Kudos
Reply

9,658 Views
Harvey021
NXP TechSupport
NXP TechSupport

@DanielDuJijun 

Have you asked customer to do DDR stress test again and with both room and high temperature? 

Due to the error in log showing rom check, pay attention to the stability of usb connection while testing.

 

Best regards

Harvey

0 Kudos
Reply

9,774 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @DanielDuJijun 

I've analyzed all logs, assume that all logs are for BSP 5.4.70 and for same board with i.MX8MM core.

According to the  202303241605.txt, then advise to check if the DDR calibration passed. if it fails, which will cause many different unforeseen boot failure, like kernel panic.

 

Best regards

Harvey

0 Kudos
Reply

9,729 Views
DanielDuJijun
Contributor III

Hi Harvey;

Thanks a lot for you support and advise.

BSP 5.4.70 and for same board with i.MX8MM core.

Yes, the BSP version is 5.4.70 and the CPU Parts : MIMX8MM6CVTKZAA,PMIC : PCA9450AAHN

EMMC : ASFC8G31M-51BIN DDR : AS4C512M16D4-75BIN.
Problem : 
1.The customer had done the DDR Calibration at room temperature and DDR stress test at high temperature. Please check the attached file "test_result_20230403-8'45'48.log" for DDR stress test at high temperature.
 
Currently, the customer feedback is that there is still a probable failure to start, please help to see if there are other suggestions and comments.
 
 
0 Kudos
Reply

9,704 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

I have checked the DDR Tool log.

There is one error log about rom_check_hab. That is a little strange.

This error has yet to happen only once. Usually this error happened during the download process.

Please check again if the error is caused by the connection cable.

From these logs, except for DDR calibration, there is file system corrupted. So If there is any specific code change for kernel or uboot by customer?

 

Best regards

Harvey

0 Kudos
Reply

9,797 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @DanielDuJijun 

Are all these boot failure for i.MX8MM but in different board and all BSP is 5.4.70?

 

Best regards

Harvey

0 Kudos
Reply