NXP DDR Test Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP DDR Test Tool

Jump to solution
6,677 Views
Arm7
Contributor II

Hello,

Arm7_0-1691620464186.png

 

Can I run this program in multiple instances on a single PC to run multiple boards ?

I have different boards and would like to run them but on a single PC.

It is possible ?

How ?

 

Thank you for you support!

0 Kudos
Reply
1 Solution
6,507 Views
bernhardfink
NXP Employee
NXP Employee

This tool is not a production test tool, it is intended to be used during the prototype phase to verify the PCB design and validate the software parameters for the DDR memory in use. In the final test of an end product you should use something like Linux memtester to verify to correct functionality of your product.

https://linux.die.net/man/8/memtester

Regards,
Bernhard.

View solution in original post

8 Replies
6,508 Views
bernhardfink
NXP Employee
NXP Employee

This tool is not a production test tool, it is intended to be used during the prototype phase to verify the PCB design and validate the software parameters for the DDR memory in use. In the final test of an end product you should use something like Linux memtester to verify to correct functionality of your product.

https://linux.die.net/man/8/memtester

Regards,
Bernhard.

6,262 Views
Arm7
Contributor II
Hello @bernhardfink

Where can I find the source or binary of the memtest ?
0 Kudos
Reply
6,218 Views
bernhardfink
NXP Employee
NXP Employee

Hi @Arm7 ,

it's "memtester" and it is open source.

https://linux.die.net/man/8/memtester

You can easily compile it for your i.MX platform in case it is not part of your BSP anyway.

$ bitbake memtester

The resulting packages (the default format is rpm) can be found inside build/tmp/deploy/rpm.

There would be an alternative to the GUI tool running on the PC. You can include a test firmware into u-boot and run it from u-boot level. Then you would have it on each board and there would be no need to load and run it from the PC.

See here:  https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/11082...

 

 

Regards,
Bernhard.


0 Kudos
Reply
6,563 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I was able to run both tests at the same time with the tool for i.MX8M.

Jorge7u7_0-1692035755115.png

But, it the case of i.MX6/7 tool, when is connected more than one board, it occurs an error.

Jorge7u7_0-1692038035558.png

Best regards.

 

0 Kudos
Reply
6,536 Views
Arm7
Contributor II

Hello, Thank you!

What about Virtual Machines, Can we run multiple virtual machines on one PC to test more boards ?

0 Kudos
Reply
6,519 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

In that case it is needed to check it, there is no information to run this tool on a VM.

Best regards.

0 Kudos
Reply
6,590 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

That feature is not in the documentation but, let me check.

Right now, I do not have access to the boards until the next Monday.

I will check with two boards (using the same processor and different processors) and I will let you know as soon as possible.

Best regards.

0 Kudos
Reply
6,583 Views
Arm7
Contributor II

Okay, thank you!

0 Kudos
Reply