NXP DDR Test Tool: ERROR: Can't open USB device!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP DDR Test Tool: ERROR: Can't open USB device!!!

2,235 Views
wonwookseo
Contributor I

Information

Processor: i.MX6 Solo

Boot Mode: Serial Download ( I checked it several times.)

USB Port: OTG Port

For SI Test, I once tried DDR Stress test with Ver. 2.8 and it worked fine with my PC.

In Device Manager in Win10, HID and USB Device popped up when USB Cable was connected to my PC.

But, an engineer said that there was the error 'Can't open USB device'.

the engineer checked device manager, but there was no HID or USB Device 

This is very weird because I once tried and it worked well but It didn't work to other PC.

Is there any driver of HID?

or what can I do in this situation?

Labels (2)
0 Kudos
Reply
1 Reply

2,116 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wonwook

one can try to attach USB Cable to another connector and

with short quality shielded cable. Also one can check if Operating System

on computer has all latest software updates.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply