NPU Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,210件の閲覧回数
_Alex_
Contributor II

Hello, 

We are trying to get NPU running on a IMX8Plus, and are often ending up with warnings about unsupported evis version. We were starting with an "imx-image-multimedia" build and adding the packagegroup-imx-ml on top of that and not having much luck. 

We ended up putting on a an imx-image-full build onto a couple systems and two of the three SOM's we had worked, but one still reported unsupported evis version when running samples. Looking into the differences we noticed the not working system had some things like "vipsi" and "dsp" in /sys/devices/platform/, but the SOM that didn't work doesn't have these. 

Any ideas as to what the minimum set of features required to get ML examples working on NPU is?
Any idea why some boards would have VIPSI/DSP and others wouldn't?

38500000.vipsi
3b6e8000.dsp 

Thanks, 

Alex

 

0 件の賞賛
返信
1 解決策
3,174件の閲覧回数
_Alex_
Contributor II

I don't totally understand what you mean by check the log about the NPU in the kernel, however we did realize that we had a mixture of SOM's with and without NPU and that was the main issue. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,184件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @_Alex_ 

Please check the log about npu in kernel 

0 件の賞賛
返信
3,175件の閲覧回数
_Alex_
Contributor II

I don't totally understand what you mean by check the log about the NPU in the kernel, however we did realize that we had a mixture of SOM's with and without NPU and that was the main issue. 

0 件の賞賛
返信