NPU Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NPU Support

Jump to solution
3,192 Views
_Alex_
Contributor II

Hello, 

We are trying to get NPU running on a IMX8Plus, and are often ending up with warnings about unsupported evis version. We were starting with an "imx-image-multimedia" build and adding the packagegroup-imx-ml on top of that and not having much luck. 

We ended up putting on a an imx-image-full build onto a couple systems and two of the three SOM's we had worked, but one still reported unsupported evis version when running samples. Looking into the differences we noticed the not working system had some things like "vipsi" and "dsp" in /sys/devices/platform/, but the SOM that didn't work doesn't have these. 

Any ideas as to what the minimum set of features required to get ML examples working on NPU is?
Any idea why some boards would have VIPSI/DSP and others wouldn't?

38500000.vipsi
3b6e8000.dsp 

Thanks, 

Alex

 

0 Kudos
Reply
1 Solution
3,156 Views
_Alex_
Contributor II

I don't totally understand what you mean by check the log about the NPU in the kernel, however we did realize that we had a mixture of SOM's with and without NPU and that was the main issue. 

View solution in original post

0 Kudos
Reply
2 Replies
3,166 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @_Alex_ 

Please check the log about npu in kernel 

0 Kudos
Reply
3,157 Views
_Alex_
Contributor II

I don't totally understand what you mean by check the log about the NPU in the kernel, however we did realize that we had a mixture of SOM's with and without NPU and that was the main issue. 

0 Kudos
Reply