NFS boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFS boot

1,533 Views
erikraynolds
Contributor IV

I'd like to do a network boot. What do I need to built image with to be enabled on i.MX8 side. How to modify (add) local.conf to enable it?

I go over quite out-dated blog Yocto NFS & TFTP boot and looking what needs to be add on target side for yocto build.

Tags (1)
0 Kudos
Reply
1 Reply

1,437 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erik

one can check Linux Guide included in Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply