U-boot flashing using JTAG on iMX8MQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot flashing using JTAG on iMX8MQ

1,590 Views
nirmalluhana
Contributor IV

Hi,

I am working on iMX8MQ based custom board.

How to I flash u-boot using JTAG interface?

For that which JTAG emulator I can use?

If there is any steps or guide available to do the same is really helpful.

Best regards,

Nirmal

Labels (1)
0 Kudos
Reply
1 Reply

1,455 Views
igorpadykov
NXP Employee
NXP Employee

Hi NIRMAL

unfortunately uboot flashing with jtag is not supported in nxp bsps,

one can try to reproduce with jtag uuu (using its sources) flashing steps:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply