NFS boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFS boot

1,521件の閲覧回数
erikraynolds
Contributor IV

I'd like to do a network boot. What do I need to built image with to be enabled on i.MX8 side. How to modify (add) local.conf to enable it?

I go over quite out-dated blog Yocto NFS & TFTP boot and looking what needs to be add on target side for yocto build.

タグ(1)
0 件の賞賛
返信
1 返信

1,425件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erik

one can check Linux Guide included in Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信