NAND Flash with i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash with i.MX6Q

Jump to solution
2,488 Views
atillametetured
Contributor V

Greetings,

On a custom hardware we are planning to add a NAND Flash on the PCB. When choosing the NAND Flash to work with i.MX6, what are

the recomended width and voltage of the NAND Flash. I am looking at Micron products. Is there an upper limit for the size of the flash regarding the

comemrcially available chips.

Regards,

Mete

Labels (2)
1 Solution
2,182 Views
art
NXP Employee
NXP Employee

Q. What are the recomended width and voltage of the NAND Flash.

A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.

Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.

A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,183 Views
art
NXP Employee
NXP Employee

Q. What are the recomended width and voltage of the NAND Flash.

A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.

Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.

A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,182 Views
atillametetured
Contributor V

Hello Artur,

Thank you very much for the detailed information.

Kind Regards,

Mete

0 Kudos
Reply