NAND Flash with i.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash with i.MX6Q

ソリューションへジャンプ
1,720件の閲覧回数
atillametetured
Contributor V

Greetings,

On a custom hardware we are planning to add a NAND Flash on the PCB. When choosing the NAND Flash to work with i.MX6, what are

the recomended width and voltage of the NAND Flash. I am looking at Micron products. Is there an upper limit for the size of the flash regarding the

comemrcially available chips.

Regards,

Mete

ラベル(2)
1 解決策
1,414件の閲覧回数
art
NXP Employee
NXP Employee

Q. What are the recomended width and voltage of the NAND Flash.

A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.

Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.

A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,415件の閲覧回数
art
NXP Employee
NXP Employee

Q. What are the recomended width and voltage of the NAND Flash.

A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.

Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.

A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,414件の閲覧回数
atillametetured
Contributor V

Hello Artur,

Thank you very much for the detailed information.

Kind Regards,

Mete

0 件の賞賛
返信