Multiple pin interrupts on same GPIO port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple pin interrupts on same GPIO port

874 次查看
ddeyo1
Contributor I

I am writing code for the M4 on an iMX8mm som.  My m4 code has 4 pins (4,5,6,7) on GPIO4 configured as interrupts.  From the documentation, it looks like interrupts 0-15 are all managed in one ISR.

Is it possible to manage multiple interrupts on the same GPIO port?

Currently when I generate two GPIO interrupts on GPIO4 I will get sometimes only get one interrupt.

Since the GPIO's are all on the same port, the priority is the same.

 

How can I configure GPIO4 to manage simultaneous interrupts on GPIO port 4?

0 项奖励
回复
1 回复

855 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

That is correct, the interrupts areOR'ed together to generate two one-bit interrupt lines:

Combined interrupt indication for GPIOx signals 0 - 15.
Combined interrupt indication for GPIOx signals 16 - 31.

It is not possible to manage simultaneous interrupts, when an interrupt condition has been met for the corresponding input signal you need to read GPIO interrupt status register to check which pin detected an interrupt and attend each interrupt per time.

Best regards.

0 项奖励
回复