Hello @Miguel04,
I am using MCUXpresso Secure Provisioning Tool. Serial download is possible through USB OTG (J9). Just have a few doubts:
I am using led_blinky project to verify. EVK is powered through USB OTG (J9) and the isolation jumper in J1 is at position 3,4. While using MCUXpresso Secure Provisioning tool to build image and write image, the SW7 switch position is kept at 01. After the Write image is successful, the SW7 switch position is changed to 10. Only after doing this switch position change, the led starts to glow.
Is this procedure correct? Why is it working only when I change the SW7 switch position from 01 to 10?