Multiple pin interrupts on same GPIO port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple pin interrupts on same GPIO port

985 Views
ddeyo1
Contributor I

I am writing code for the M4 on an iMX8mm som.  My m4 code has 4 pins (4,5,6,7) on GPIO4 configured as interrupts.  From the documentation, it looks like interrupts 0-15 are all managed in one ISR.

Is it possible to manage multiple interrupts on the same GPIO port?

Currently when I generate two GPIO interrupts on GPIO4 I will get sometimes only get one interrupt.

Since the GPIO's are all on the same port, the priority is the same.

 

How can I configure GPIO4 to manage simultaneous interrupts on GPIO port 4?

0 Kudos
Reply
1 Reply

966 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

That is correct, the interrupts areOR'ed together to generate two one-bit interrupt lines:

Combined interrupt indication for GPIOx signals 0 - 15.
Combined interrupt indication for GPIOx signals 16 - 31.

It is not possible to manage simultaneous interrupts, when an interrupt condition has been met for the corresponding input signal you need to read GPIO interrupt status register to check which pin detected an interrupt and attend each interrupt per time.

Best regards.

0 Kudos
Reply