Multiple endpoints using RPMsg RTOS Layer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple endpoints using RPMsg RTOS Layer

3,955 次查看
rlumo
Contributor II

Does the RPMsg RTOS Layer's create endpoint (rpmsg_rtos_create_ept) supports multiple endpoints?

0 项奖励
回复
2 回复数

3,827 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Roger

>Does the RPMsg RTOS Layer's create endpoint (rpmsg_rtos_create_ept) supports multiple endpoints?

no. Sorry NXP i.MX releases do not support multiple endpoints.

For multiple endpoints example one can look at

Asymmetric Multiprocessing: RPMsg – Linux/Android | Kynetics 

Asymmetric Multiprocessing - Boundary Devices Nitrogen7 | Kynetics 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,708 次查看
enricorocheti_
Contributor III

Hello @igorpadykov, RPMsg in the NXP SDK (I'm using the RT1160EVK) still don't support multiple endpoints? 

I was thinking about creating two endpoints in my cores, one channel to send/recv synchronous messages and the other to send/recv asynchronous messages.

Thank you,

Enrico

0 项奖励
回复