MIMX8ML8DVNLZAB || GPIO Mapping sheet, Thermal Sheet and IBIS Model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMX8ML8DVNLZAB || GPIO Mapping sheet, Thermal Sheet and IBIS Model

2,002件の閲覧回数
JyotiVaishnav
Contributor II

Hello NXP Team,


We are designing a hardware platform using MIMX8ML8DVNLZAB processor. 

Can you please share a GPIO mapping sheet, Thermal Data and IBIS Model of the processor for our reference. 

0 件の賞賛
返信
5 返答(返信)

1,974件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav,

I hope you are doing well.

1. GPIO Mapping Sheet
NXP does not have any specific GPIO mapping sheet. However, one can download the Config Tools for i.MX Applications Processors and perform pin muxing for the MIMX8ML8DVNLZAB processor. One can also find the pin muxing file of the i.MX8MP EVK in this tool.

2. Thermal Data
There is no specific thermal data available. One can refer to Section 6 Thermal Considerations of i.MX 8M Plus Hardware Developer’s Guide and perform board-level thermal analysis.

2. IBIS Model
One can download the IBIS model from the link given below:
i.MX 8M Plus 15x15 IBIS Model

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

1,943件の閲覧回数
JyotiVaishnav
Contributor II

Hello @riteshmpatel 


Hope you are doing well !!

Thanks for the information. 

Can you please share below temperature details for thermal simulation. 

  • Ambient Temperature
  • Operating Temperature
  • Storage Temperature
  • Case Temperature
  • Junction Temperature
  • Junction to Board Temperature
  • Junction to Case Temperature
  • Junction to Ambient Temperature
Please share a Layer Stack up also.
0 件の賞賛
返信

1,932件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav,

Please see the required details below which can be provided by us:

- Junction temperature can be considered the same which can be found in Table 12. Operating ranges in the i.MX8MP datasheet.

- Storage temperature can be found in Table 9. Absolute maximum ratings in the i.MX8MP datasheet.

- Thermal resistance data can be found in Section 3.1.2 Thermal resistance in the i.MX8MP datasheet.

- For the Layer stack up of the SoM board, one can refer to PCB Layout of i.MX 8M Plus LPDDR4 EVK Compute Module Design Files

- For the Layer stack up of the Baseboard, one can refer to PCB Layout of i.MX 8M Plus EVK Base Board Design Files.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

1,915件の閲覧回数
JyotiVaishnav
Contributor II

Hello @riteshmpatel 

Thanks for the information. 

Below details are not there, can you please check once again and provide the details. 

  • Ambient Temperature
  • Operating Temperature
  • Case Temperature
  • Junction to Board Temperature
0 件の賞賛
返信

1,893件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav,

- Ambient temperature would depend upon your application.

- The operating temperature is the same as the junction temperature.

- Case temperature can be calculated by using the Junction to Case Thermal Resistance value mentioned in the datasheet. and power dissipation value (as per your application).

- Junction to Board Temperature data is not available.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信