Multiple WiFi interfaces

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple WiFi interfaces

1,238件の閲覧回数
petersteinberg
Contributor I

I've got custom boards that need to support wireless Ethernet either via an on-board wireless module or through a USB wireless interface.

Everything works as I expect when only one of the interfaces is present.

When I boot the board with the on-board wireless module and a USB wireless interface attached the on-board module is loaded as wlan1 and the USB interface is loaded as wlan0.

I really want to have the on-board module always identify as wlan0.

Any ideas on what I need to change to always force the on-board module to load as wlan0 if it is present?

Our kernel is based on Marshmallow (git tag android-6.0.1_r22), kernel 4.1.15.

Thanks,
  Peter Steinberg

ラベル(1)
0 件の賞賛
返信
0 返答(返信)