Multiple Cameras on iMX7D MIPI-CSI interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple Cameras on iMX7D MIPI-CSI interface

6,801 次查看
dogisfat
Contributor IV

Is it possible to connect multiple MIPI cameras to the iMX7D MIPI-CSI interface using the virtual channels and capture from both cameras simultaneously?

标签 (2)
0 项奖励
回复
3 回复数

5,061 次查看
Richard1z
Contributor II

The referenced document says:

- CSI can support up to one 24-bit parallel camera interface.

- MIPI CSI-2 Controller and PHT support 2 data lanes and 1 clock lane.

I imagine the question relates to the connecting of 2 MIPI CSI2 serial cameras. Is this possible ?

Richard.

0 项奖励
回复

5,061 次查看
igorpadykov
NXP Employee
NXP Employee

for  virtual channels usage please refer to link

4 video capture using MIPI-CSI2 port 

and file MIPI CSI-Memory flow.pdf on that link

CMOS Sensor Interface (CSI) is parallel interface and only

one camera can be connected to it.

Best regards
igor

0 项奖励
回复

5,061 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Al

yes possible as described in sect.13.5.1.1 Features i.MX7D RM :

Support four channel virtual channels

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复