Multimedia tests of GTS are failing on i.MX6 running Android 7.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multimedia tests of GTS are failing on i.MX6 running Android 7.1.1

1,637 Views
saiyamdoshi
Contributor II

Hello,

We are using i.MX6QDL based custom board running Android 7.1.1. On this device when executing GTS tests, we are observing failures related to audio/video playback tests as below. 

armeabi-v7a GtsMediaTestCases
TestResultDetails
com.google.android.media.gts.WidevineDashPolicyTests#testL30SLicense20SPlayback
fail
java.lang.Exception: Failed components: < Audio Not Reached Seconds > < Expect Exceptions >

armeabi-v7a GtsExoPlayerTestCases
TestResultDetails
com.google.android.exoplayer.gts.DashTest#testH264AdaptiveWithRendererDisabling
fail
junit.framework.
AssertionFailedError: Test timed out after 300000 ms.

Also attached the logcat logs. Please provide your input on what could be the issue.

Thanks.

1 Reply

1,334 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

 

Is there a possibility that you can upgrade to our newer Android version (7.1.2)?

 

Some errors were fixed in that version, probably in that version the GTS test pass.

Best Regards,

Diego.

0 Kudos
Reply