Multimedia tests of GTS are failing on i.MX6 running Android 7.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multimedia tests of GTS are failing on i.MX6 running Android 7.1.1

1,612 次查看
saiyamdoshi
Contributor II

Hello,

We are using i.MX6QDL based custom board running Android 7.1.1. On this device when executing GTS tests, we are observing failures related to audio/video playback tests as below. 

armeabi-v7a GtsMediaTestCases
TestResultDetails
com.google.android.media.gts.WidevineDashPolicyTests#testL30SLicense20SPlayback
fail
java.lang.Exception: Failed components: < Audio Not Reached Seconds > < Expect Exceptions >

armeabi-v7a GtsExoPlayerTestCases
TestResultDetails
com.google.android.exoplayer.gts.DashTest#testH264AdaptiveWithRendererDisabling
fail
junit.framework.
AssertionFailedError: Test timed out after 300000 ms.

Also attached the logcat logs. Please provide your input on what could be the issue.

Thanks.

1 回复

1,309 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

 

Is there a possibility that you can upgrade to our newer Android version (7.1.2)?

 

Some errors were fixed in that version, probably in that version the GTS test pass.

Best Regards,

Diego.

0 项奖励
回复