Multi-Byte Read from i.MX 6 MIPI Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi-Byte Read from i.MX 6 MIPI Controller

1,524件の閲覧回数
aditya_rm
Contributor I

Hi,

I'm trying to read multiple bytes of data from a MIPI/DSI driver IC. I can send a command to read up to four bytes correctly but requesting to read any parameter that returns more than four bytes from the driver IC causes it to return zeroes. Other test equipment that I have that can be used to control the driver confirms that the problem is not with the driver. Am I missing something at my end?

For reference, my application is bare-metal and does not use Linux and runs on an i.MX 6Solo processor.

Thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,408件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

what MIPI/DSI interface used in the case, for DBI one can look on

MIPI DBI support on i.MX6 Solo 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信