How to visualize the boot process using bootchart?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to visualize the boot process using bootchart?

2,811 Views
suhaskaundinya
Contributor I

Hello,

I am using i.MX 6Quad SABRE-AI with Andriod N.

I need to visualize the boot process and the time it takes to boot up.

Could someone tell me how to use bootchart for this? Also if any other visualizer is available, let me know.

Best Regards,

Suhas

Labels (3)
0 Kudos
Reply
1 Reply

1,560 Views
igorpadykov
NXP Employee
NXP Employee

Hi Suhas

I am afraid there is no way to check or visualize rom boot flow,

in uboot one can add gpio toggle codes in uboot/board/freescale/mx6qsabreauto/mx6qsabreauto.c

or plugin.s.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply