Mouse cursor is not showing up in overlay buffer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mouse cursor is not showing up in overlay buffer

1,125 次查看
arunmenon
Contributor I

I am running my QT application in overly buffer( /dev/fb1) of freescale board(IMX-6).

Before starting application I have selected fb1 & unblank b1 and my application is working fine in overlay buffer.

But, some times mouse cursor is not showing up when application is started in overlay buffer( frequency of the issue is very less) and i need to reconnect my usb mouse on board.

Do I need to unset QT_QPA_EGLFS_HIDECURSOR  environment ?

or set QT_QPA_EVDEV_MOUSE_PARAMETERS.

------------------------------------------------------------------------------------------------------------------------------

Update:

Now, I have used QT_QPA_EGLFS_HIDECURSOR  and  QT_QPA_EVDEV_MOUSE_PARAMETERS.

Still some times mouse cursor is not showing up. Any help will be appreciated

Regards,

Arun

标签 (3)
0 项奖励
回复
0 回复数