Motion Control using iMX7 SoM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motion Control using iMX7 SoM

1,497件の閲覧回数
DeepakKukreja
Contributor III

I am using the iMX7 Dual SoM from Toradex in a design. I wish to generate PUL/DIR control signals for controlling a servo motor from this. The reference manual mentions the FlexTimer Module as well as a PWM module separately.

While the Flextimer module mentions that it can be used to generate PWM signals for motor control, the PWM sections mentions that it has been optimized to generate Audio.

So what should I refer to if I need to generate motion profiles to control a servo motor.

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
Pavel
NXP Employee
NXP Employee

It looks like that your servo motor is step-motor.

This motor requires generates various frequency for signal PUL. Maximum frequency for step motors is 1000Hz - 5000Hz.

Usually Flextimer module or system timer is used for this task.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信