More UART connectivity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

More UART connectivity

2,336件の閲覧回数
jupiter_hce
Contributor III

Hi,iMX6ULZ

I am currently running Linux on iMX6ULZ SoC 4 x UART but I need one or two more UART, which iMX6 or iMX7 SoC I can select? I can use the NXP MFGTools to flash image to iMX6ULZ NAND, will the same tools compatible for all other iMX6 or iMX7 SoC?

Thank you.

Kind regards,

jhiMX6ULZ

0 件の賞賛
返信
3 返答(返信)

2,258件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

one can look at i.MX6 comparison table

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,258件の閲覧回数
jupiter_hce
Contributor III

Hi igor,

Thanks for the response and the link, but there are more discrepancies between the two documents, in the document  i.MX 6ULZ Applications Processors that the number of UART is 4 which I think is correct, where the FLYRIMXPRDCMPR.pdf that the number of UART is 8 which I think is wrong, could you please further clarify it?

Thank you.

FLYRIMXPRDCMPR.pdf 

 

Kind regards.

0 件の賞賛
返信

2,258件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

 

you are right, correct number of UART is 4 .

 

Best regards
igor

0 件の賞賛
返信