The 3.0USB port of the IMX8MM PCIE extension is not recognized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The 3.0USB port of the IMX8MM PCIE extension is not recognized

891 Views
2546029096
Contributor I

Hello, I'm having some problems.When I used the IMX8MM chip, I extended two 3.0USB ports in the PCIE bus via a D720202 chip.But the two extended 3.0USB ports only ran at 2.0 speeds, and when I tested the pins with an oscilloscope, I found that the read/write data was running over a 2.0 circuit

0 Kudos
Reply
3 Replies

799 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Toby,

i.MX8MM CPU supports USB2.0, don't support USB3.0.

so the result you measured is no problem.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply

799 Views
2546029096
Contributor I

Yes ,I know the iMX8MM CPU supports USB2.0,don`t support USB3.0. But the question I want to ask is whether the CPU supports 3.0USB via PCIE extension

Thank!

0 Kudos
Reply

799 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Toby,

>>But the question I want to ask is whether the CPU supports 3.0USB via PCIE extension

If your purpose is :  I.MX8MM PCIe --- > PCIe To USB3.0 bridge---->USB3.0 interface for application.

It should be no problem.

BUT if you find the bridge is working in USB 2.0 mode, you can contact the provider of the bridge to ask for help. Because on CPU side, we only give you some help on PCIe.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply