More UART connectivity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

More UART connectivity

2,333 次查看
jupiter_hce
Contributor III

Hi,iMX6ULZ

I am currently running Linux on iMX6ULZ SoC 4 x UART but I need one or two more UART, which iMX6 or iMX7 SoC I can select? I can use the NXP MFGTools to flash image to iMX6ULZ NAND, will the same tools compatible for all other iMX6 or iMX7 SoC?

Thank you.

Kind regards,

jhiMX6ULZ

0 项奖励
回复
3 回复数

2,255 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

one can look at i.MX6 comparison table

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,255 次查看
jupiter_hce
Contributor III

Hi igor,

Thanks for the response and the link, but there are more discrepancies between the two documents, in the document  i.MX 6ULZ Applications Processors that the number of UART is 4 which I think is correct, where the FLYRIMXPRDCMPR.pdf that the number of UART is 8 which I think is wrong, could you please further clarify it?

Thank you.

FLYRIMXPRDCMPR.pdf 

 

Kind regards.

0 项奖励
回复

2,255 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

 

you are right, correct number of UART is 4 .

 

Best regards
igor

0 项奖励
回复