Module for MIPI DSI not built with yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Module for MIPI DSI not built with yocto

1,985件の閲覧回数
vinaykumarvepur
Contributor I

Display - TFT3p5581-E(MIPI DSI)

Board - mcimx7sabre dual

I have enabled MIPI DSI module through menuconfig for mcimx7sabre dual and built linux from yocto.

After the modules are built I could find only mxc_dcic.ko under drivers/video/fbdev/mxc/ but couldn't find mxc_mipi_dsi_samsung.ko .

Is mxc_mipi_dsi_samsung.ko is the required module or is it integrated in mxc_dcic.ko only? And more over in kernel bootup it is saying "mxsfb 30730000.lcdif: failed to find mxc display driver"

Please help me in getting this display work.

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

1,762件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinal

mipi-dsi driver is described in sect.7.2.1 MIPI DSI IP Driver Software Operation

attached Linux Manual. Recommended to try nxp bsps from

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga

Demo Images

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX6UL7D&appType=license&location=null 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信