Missing iMX 8M Mini support for Media controller API

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing iMX 8M Mini support for Media controller API

1,817 Views
krzysztof_kozlo
Contributor II

Hi,

I am using iMX 8M Mini with several MIPI CSI sensors (OV, IMX). The Linux kernel is based on codeaurora imx_4.19.35_1.1.0 (v4.19.35-5188-g8507afc3a397).

It's very important to have the media controller API available and use media-ctl however iMX 8M Mini is not supported. Other flavors are (fsl,imx8mn, fsl,imx8qxp, fsl,imx8qxp) but the "mm" is not.

Since it is a basic feature of MIPI CSI of SoC, it's crucial to have it available.

When could we expect adding missing media controller API support for i.MX 8 M Mini? Or maybe there is some workaround for this?

Best regards,

Krzysztof

Labels (2)
0 Kudos
Reply
1 Reply

1,780 Views
igorpadykov
NXP Employee
NXP Employee

Hi Krzysztof

VPI APIs are described in nxp official linux documentation, for example

 i.MX VPU API Reference Manual

Also one can look Chapter 6 Video i.MX Linux Reference Manual

Supported functionalities are described in i.MX Linux Release Notes

I am afraid  media-ctl is not supported by nxp.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply