Mismatch of reset value in i.MX27

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mismatch of reset value in i.MX27

Jump to solution
2,083 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about the reset value in i.MX27.

I read chapter 3 of MCIMX27 Multimedia Applications Processor Reference Manual (MCIMX27RM Rev. 0.4 06/2012).

Q1

0x1002_700C (SPCTL0) SPLL Control Register 0
The reset value of Table 3-4 and Figure 3-7 doesn't match. Which is correct ?

Q2

0x1002_7018 (PCDR0) Peripheral Clock Divider Register 0
The reset value of Table 3-4 and Figure 3-10 doesn't match. Which is correct ?

Q3

0x1002_701C (PCDR1) Peripheral Clock Divider Register 1
The reset value of Table 3-4 and Figure 3-11 doesn't match. Which is correct ?

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
1,946 Views
joanxie
NXP TechSupport
NXP TechSupport

pls see the page 1724 of Reference Manual,

3.4, 3-9
In Table 3-4, “PLL Clock Controller Memory Map,” update the Reset Value

View solution in original post

0 Kudos
Reply
7 Replies
1,946 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the mx27RM rev0.4,  I don't find any different value, SPCTL0 is 0x84FF_1C53, PCDR0 is 0x1204_10C3, PCDR1 is 0x0303_0303.

0 Kudos
Reply
1,946 Views
ko-hey
Senior Contributor II

According to the Table 3-4, the reset value is as follow.

However, description of each register reset value is not match.

Could you check again ?

image001.png

0 Kudos
Reply
1,946 Views
ko-hey
Senior Contributor II

joanxie

Could you follow the question ?

Ko-hey

0 Kudos
Reply
1,947 Views
joanxie
NXP TechSupport
NXP TechSupport

pls see the page 1724 of Reference Manual,

3.4, 3-9
In Table 3-4, “PLL Clock Controller Memory Map,” update the Reset Value
0 Kudos
Reply
1,946 Views
ko-hey
Senior Contributor II

Joan Xie

As a result, the Table 3-4 is correct value.

Am I correct ?

Ko-hey

0 Kudos
Reply
1,946 Views
joanxie
NXP TechSupport
NXP TechSupport

Reference Manual I sent to you has two table 3-4, do you mind opending the link I sent ,then you would know what I mean.

0 Kudos
Reply
1,946 Views
ko-hey
Senior Contributor II

Hi Joan Xie

I understood there are two table 3-4 and the table 3-4 of section 3-4, 3-9 is same as the each register's detail description.

Thank you for your support.

Ko-hey

0 Kudos
Reply