Mipi OLED interface errors after interfacing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mipi OLED interface errors after interfacing

5,735件の閲覧回数
kunalkulshresth
Contributor III

Dear Team,

 

I need help while I try to interface a 400x400 round OLED to iMX6. Attaching the logs and datasheet. Please let me know the points which could be wrong.

 

I have attached the mxcfb_hx8369_wvga.c which I am using and the Init code file which I have received from manufacturer. I also am looking forward to know if the lcd_setup function in mxcfb_hx8369_wvga.c looks ok. How to I write the data to registers as is expected in the pdf of init code?

 

Any help will be great.

 

 

&mipi_dsi {
    compatible = "fsl,imx6dl-mipi-dsi";
    reg = <0x021e0000 0x4000>;
    interrupts = <0 102 0x04>;
    gpr = <&gpr>;
    clocks = <&clks 138>, <&clks 204>;
    clock-names = "mipi_pllref_clk", "mipi_cfg_clk";
    dev_id = <0>;
    disp_id = <0>;
    lcd_panel = "TRULY-WVGA";
    disp-power-on-supply = <&reg_mipi_dsi_pwr_on>;
    resets = <&mipi_dsi_reset>;
    status = "okay";
};

 

    mipi_dsi_reset: mipi-dsi-reset {
        compatible = "gpio-reset";
        reset-gpios = <&gpio5 15 GPIO_ACTIVE_LOW>;
        reset-delay-us = <50>;
        #reset-cells = <0>;
    };

 

    reg_mipi_dsi_pwr_on: mipi_dsi_pwr_on {
        compatible = "regulator-fixed";
        regulator-name = "mipi_dsi_pwr_on";
        gpio = <&gpio6 14 0>;
        enable-active-high;
    };

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

U-Boot 2014.04 (Jan 04 2017 - 21:04:41)

 

CPU:   Freescale i.MX6DL rev1.2 at 792 MHz
Reset cause: POR
Board: MX6-Sabreauto revA
I2C:   ready
DRAM:  2 GiB
NAND:  0 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
Found PFUZE100! deviceid=10,revid=12
mmc1 is current device
Net:   FEC [PRIME]
Normal Boot
Hit any key to stop autoboot:  0
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5933744 bytes read in 276 ms (20.5 MiB/s)
Booting from mmc ...
reading imx6dl-sabreauto.dtb
43719 bytes read in 19 ms (2.2 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x5a8ab0 ]
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800dac6

 

Starting kernel ...

 

Booting Linux on physical CPU 0x0
Linux version 3.14.28-1.0.0_ga+g91cf351 (kunalk@Linux2-tds) (gcc version 4.9.1 (GCC) ) #21 SMP PREEMPT Mon Apr 10 19:49:36 IST 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 DualLite/Solo SABRE Automotive Board
cma: CMA: reserved 320 MiB at 6a000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @ee72d000 s8896 r8192 d15680 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 520720
Kernel command line: console=ttymxc3,115200 root=/dev/mmcblk2p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 1736120K/2097152K available (7217K kernel code, 394K rwdata, 6144K rodata, 328K init, 428K bss, 361032K reserved, 270336K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
    lowmem  : 0x80000000 - 0xef800000   (1784 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x80d146c4   (13362 kB)
      .init : 0x80d15000 - 0x80d672c0   ( 329 kB)
      .data : 0x80d68000 - 0x80dcab40   ( 395 kB)
       .bss : 0x80dcab4c - 0x80e35e1c   ( 429 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 512 kB
failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x106de8e0 - 0x106de938
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated.
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6DL, silicon rev 1.2
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1100 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2400 mV
vddarm: 725 <--> 1450 mV at 1150 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6qdl-sabreauto/audmux
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
cs42888_supply: 3300 mV
3P3V: 3300 mV
vio1: 3300 mV
vio2: 3300 mV
vd: 3300 mV
va: 5000 mV
platform usb_h1_vbus.28: Driver reg-fixed-voltage requests probe deferral
platform usb_otg_vbus.29: Driver reg-fixed-voltage requests probe deferral
mipi_dsi_pwr_on: no parameters
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usbphy_nop1.12 supply vcc not found, using dummy regulator
usbphy_nop2.13 supply vcc not found, using dummy regulator
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.18
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 4, 65536 bytes)
TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP: reno registered
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
bounce pool size: 64 pages
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) ������ 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 3502
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
backlight.17 supply power not found, using dummy regulator
ldb ldb.15: crtc not specified or invalid
ldb: probe of ldb.15 failed with error -22
Before Device Reset
After Device Reset ret = 0
mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
imx6dl-pinctrl 20e0000.iomuxc: pin MX6DL_PAD_DISP0_DAT21 already requested by 20e0000.iomuxc; cannot claim for lcd.24
imx6dl-pinctrl 20e0000.iomuxc: pin-58 (lcd.24) status -22
imx6dl-pinctrl 20e0000.iomuxc: could not request pin 58 (MX6DL_PAD_DISP0_DAT21) from group ipu1grp-1  on device 20e0000.iomuxc
mxc_lcdif lcd.24: Error applying setting, reverse things back
imx6dl-pinctrl 20e0000.iomuxc: pin MX6DL_PAD_DISP0_DAT21 already requested by 20e0000.iomuxc; cannot claim for lcd.24
imx6dl-pinctrl 20e0000.iomuxc: pin-58 (lcd.24) status -22
imx6dl-pinctrl 20e0000.iomuxc: could not request pin 58 (MX6DL_PAD_DISP0_DAT21) from group ipu1grp-1  on device 20e0000.iomuxc
mxc_lcdif lcd.24: Error applying setting, reverse things back
mxc_lcdif lcd.24: can't get/select pinctrl
mxc_lcdif: probe of lcd.24 failed with error -22
mxc_sdc_fb fb.23: registered mxc display driver mipi_dsi
Console: switching to colour frame buffer device 50x25
imx_epdc_fb 20f4000.epdc: can't get/select pinctrl
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 1, Metal layer: 2
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1375 mV
SW1C: 300 <--> 1875 mV at 1375 mV
SW2: 800 <--> 3300 mV at 3000 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 1975 mV at 1800 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 800 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 1800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 2500 mV
VGEN6: 1800 <--> 3300 mV at 2800 mV
Serial: IMX driver
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
console [ttymxc3] enabled
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
si476x-core 1-0063: Using default platform data.
si476x-core 1-0063: No IRQ number specified, will use polling
si476x-core 1-0063: Error while sending command 0x11
si476x-core 1-0063: The device in inconsistent power state
CAN device driver interface
2094000.can supply xceiver not found, using dummy regulator
flexcan 2094000.can: device registered (reg_base=f01c0000, irq=143)
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517
platform 2184000.usb: Driver imx_usb requests probe deferral
imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517
platform 2184200.usb: Driver imx_usb requests probe deferral
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
2-0044 supply vdd not found, using dummy regulator
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
mxc_v4l2_output v4l2_out.32: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.32: V4L2 device registered as video17
2-000e supply vdd not found, using dummy regulator
2-000e supply vddio not found, using dummy regulator
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
2-001c supply vdd not found, using dummy regulator
2-001c supply vddio not found, using dummy regulator
mma8451 2-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 2-001c failed with error -22
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
Bluetooth: Generic Bluetooth SDIO driver ver 0.1
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
galcore: clk_get vg clock failed, disable vg!
Galcore version 5.0.11.25762
mmc2: new ultra high speed DDR50 SDHC card at address 0007
mmcblk2: mmc2:0007 SS08G 7.21 GiB
 mmcblk2: p1 p2
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_vpu 2040000.vpu: VPU initialized
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a160100 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 3e 6c 10 93 0f cb 9a 1c
platform caam_sm: [0008] f7 82 ca 3a 42 52 1e 19
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 0b 12 03 60 38 fe eb 6b
platform caam_sm: [0008] 51 ec 7b ff 91 d0 8e d7
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 50 0d f6 ae 32 c7 3b a0
platform caam_sm: [0008] 6c db fb 85 c5 c9 7d b1
platform caam_sm: [0016] a8 b5 42 7a 45 67 74 c2
platform caam_sm: [0024] 37 c7 f3 4a 2b b3 b5 24
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 2e b2 86 8c 6c 5c 6f 43
platform caam_sm: [0008] 34 18 3f 7c 84 1a e8 72
platform caam_sm: [0016] 8f fa 01 95 4b ab 46 16
platform caam_sm: [0024] c1 20 e1 dc 98 fc 6a 4b
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 1c be 68 36 79 8f 44 cf
platform caam_sm: [0008] b5 49 58 c9 23 65 a0 29
platform caam_sm: [0016] af e2 0a bb 6d a2 af 9b
platform caam_sm: [0024] 2e 2a 88 22 6a 7e 11 36
platform caam_sm: [0032] 99 73 cd de c5 5e c8 e4
platform caam_sm: [0040] 0f 49 65 10 52 f3 86 d5
platform caam_sm: [0048] 70 7d fe 86 98 37 e6 13
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] ab 62 68 c4 15 95 9e 35
platform caam_sm: [0008] 78 83 bf 9d 97 ac 66 f4
platform caam_sm: [0016] 6c 13 c2 d7 cd 6a a0 a4
platform caam_sm: [0024] 17 9e 6b fa 2a a0 3d 92
platform caam_sm: [0032] 07 70 43 0c 3c ee 86 80
platform caam_sm: [0040] 36 e5 09 ef 51 29 1e 4b
platform caam_sm: [0048] 8e f9 20 4a e4 2e bd 2d
platform caam_sm: [0056] 0d 0c ce c2 29 58 4d e9
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 1f 20 32 de 1d b5 9e 90
platform caam_sm: [0008] 85 bb e8 d7 ff b0 b5 74
platform caam_sm: [0016] b5 85 f0 b3 43 65 a1 b6
platform caam_sm: [0024] 90 43 67 96 79 af d4 c9
platform caam_sm: [0032] 57 88 f1 33 13 60 25 76
platform caam_sm: [0040] ab 3b 25 87 c3 af 1c c1
platform caam_sm: [0048] 67 00 fd 5d c9 86 1f 94
platform caam_sm: [0056] c9 01 d9 c3 a4 65 8a 7f
platform caam_sm: [0064] 14 25 64 33 33 1c 6d 59
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 8e ab 05 f6 21 6c 90 b8
platform caam_sm: [0008] 1c 99 ce 31 87 d2 2a fc
platform caam_sm: [0016] fd 99 79 64 78 be 53 2a
platform caam_sm: [0024] 03 49 bc ed 71 10 31 09
platform caam_sm: [0032] a8 4e ee 8c dd c8 06 8b
platform caam_sm: [0040] a8 ee eb 01 99 ac e9 14
platform caam_sm: [0048] 1a 4d de 82 57 84 e1 61
platform caam_sm: [0056] 85 7a 55 9f 68 8c 06 c2
platform caam_sm: [0064] 53 86 b0 b0 c0 f5 17 28
platform caam_sm: [0072] d4 55 db 1e 8c 79 a1 9f
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 74 aa e3 98 f9 99 48 71
platform caam_sm: [0008] fe 58 60 e2 8f 95 3d 29
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 0b 12 03 60 38 fe eb 6b
platform caam_sm: [0008] 51 ec 7b ff 91 d0 8e d7
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 50 0d f6 ae 32 c7 3b a0
platform caam_sm: [0008] 6c db fb 85 c5 c9 7d b1
platform caam_sm: [0016] 18 ab 4a b8 38 b0 d9 80
platform caam_sm: [0024] 48 fb 2f 2f 53 72 79 50
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 2e b2 86 8c 6c 5c 6f 43
platform caam_sm: [0008] 34 18 3f 7c 84 1a e8 72
platform caam_sm: [0016] 8f fa 01 95 4b ab 46 16
platform caam_sm: [0024] c1 20 e1 dc 98 fc 6a 4b
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
cs42xx8 1-0048: failed to get device ID, ret = -5
cs42xx8: probe of 1-0048 failed with error -5
fsl-asrc 2034000.asrc: driver registered
fsl-hdmi-dai hdmi_audio.3: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of hdmi_audio.3 failed with error -12
imx-cs42888 sound-cs42888.25: failed to find codec platform device
imx-cs42888: probe of sound-cs42888.25 failed with error -22
imx-spdif sound-spdif.20: snd-soc-dummy-dai <-> 2004000.spdif mapping ok
imx-audio-hdmi sound-hdmi.21: initialize HDMI-audio failed. load HDMI-video first!
imx-tuner-si476x sound-fm.30: failed to find FM platform device
imx-tuner-si476x: probe of sound-fm.30 failed with error -22
NET: Registered protocol family 26
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
failed to disable 1.2 GHz OPP
VGEN2: disabling
SWBST: disabling
SW4: disabling
regulator-dummy: disabling
imx mcc test is registered.
usb_h1_vbus: 5000 mV
usb_otg_vbus: 5000 mV
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
input: gpio-keys.18 as /devices/soc0/gpio-keys.18/input/input1
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
ALSA device list:
  #0: imx-spdif
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk2p2): using internal journal
EXT3-fs (mmcblk2p2): recovery complete
EXT3-fs (mmcblk2p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 328K (80d15000 - 80d67000)
INIT: version 2.88 booting
Starting udev
udevd[177]: starting version 182
ERROR: v4l2 capture: slave not found!
FAT-fs (mmcblk2p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
bootlogd: cannot allocate pseudo tty: No such file or directory
random: dd urandom read with 81 bits of entropy available
ALSA: Restoring mixer settings...
No state is present for card imxspdif
Found hardware: "imx-spdif" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card imxspdif
Fri Feb  3 11:37:18 UTC 2017
INIT: Entering runlevel: 5
Configuring network interfaces... fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
done.
Starting Xserver
Starting system message bus: dbus.
Starting Connection Manager
Starting Dropbear SSH server: dropbear.
Starting rpcbind daemon...done.
mipi_dsi 21e0000.mipi:          write_reg:0x04, val:0x00000000.
mipi_dsi 21e0000.mipi:          write_reg:0x54, val:0x00000000.
mipi_dsi 21e0000.mipi:          write_reg:0x08, val:0x00000107.
mipi_dsi 21e0000.mipi:          write_reg:0x0c, val:0x000000e0.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
^Cmipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
^Cmipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
^Cmipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
^Cmipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
^Cmipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: mipi_dsi IRQ status0:0x0, status1:0x80!
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x44, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x48, val:0x00000080.
mipi_dsi 21e0000.mipi: read_reg:0x50, val:0x00000000.
mipi_dsi 21e0000.mipi: read_reg:0x4c, val:0x00000000.

 

CPU:   Temperature 27 C, calibration data: 0x5b34fa7d

Original Attachment has been moved to: mxcfb_hx8369_wvga.c.zip

0 件の賞賛
返信
2 返答(返信)

5,061件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kunal

please check attached Linux Manual Chapter 7 MIPI DSI Driver.

For 400x400 resolution fb_videomode truly_lcd_modedb[], mxcfb_hx8369_wvga.c

should be customized with new panel timings. Also manufacturer init code

should be placed in mipid_hx8369_lcd_setup().

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,061件の閲覧回数
kunalkulshresth
Contributor III

Hi Igor,

Thanks. I have tried to configure these functions as per datasheet of oled. Any idea how to test the fb linked with Mipi interface working? I mean I want to quickly try with a test that tries to show some dummy image on the OLED. Please let me know if there are some relevant tests to verify mipi interface. I tested using DSO, the clock and data line show some movement but oled display still black. Need help.

Thanks and regards,

Kunal

0 件の賞賛
返信