Debug UART as Application UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug UART as Application UART

Jump to solution
2,245 Views
adityapatil
Contributor II

HI,

I am using im283 cpu and would like to know whether the debug UART can be made to function as application

-Thanks

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
2,105 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here you can try Disable serial console in kernel, remove kernel argument (console=XXX) from kernel command line. If you still need a console, try telnet, ssh through ethernet. Hope this can help you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,106 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here you can try Disable serial console in kernel, remove kernel argument (console=XXX) from kernel command line. If you still need a console, try telnet, ssh through ethernet. Hope this can help you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,105 Views
adityapatil
Contributor II

Hi,

Thanks for the reply 

-Aditya

0 Kudos
Reply