Minimization power consumption by changing the register settings of unused pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimization power consumption by changing the register settings of unused pins

Jump to solution
1,591 Views
ko-hey
Senior Contributor II

Hi all

My customer want to minimize power consumption.

Can user reduce the power consumption by changing the register settings of unused pins ?

Do you have any information for it ?

I have already read following application note but can't find a such information.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
1,464 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

seems for unused pins one can only try to change/disable pull resistors

or set it as open drain (bit ODE register IOMUXC_SW_PAD_CTL_PAD_x_y).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,465 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

seems for unused pins one can only try to change/disable pull resistors

or set it as open drain (bit ODE register IOMUXC_SW_PAD_CTL_PAD_x_y).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,464 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick reply.

Let me confirm the meaning of your following comment.

seems for unused pins one can only try to change/disable pull resistors

What is the meaning of the pull resistors ?

I think that the pull resistor means PKE field.

Is it correct ?

Ko-hey

1,464 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes correct

Best regards

igor

0 Kudos
Reply
1,464 Views
ko-hey
Senior Contributor II

Hi Igor

Thanks !

Ko-hey

0 Kudos
Reply