Minimization power consumption by changing the register settings of unused pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimization power consumption by changing the register settings of unused pins

ソリューションへジャンプ
1,603件の閲覧回数
ko-hey
Senior Contributor II

Hi all

My customer want to minimize power consumption.

Can user reduce the power consumption by changing the register settings of unused pins ?

Do you have any information for it ?

I have already read following application note but can't find a such information.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

Ko-hey

ラベル(1)
0 件の賞賛
返信
1 解決策
1,476件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

seems for unused pins one can only try to change/disable pull resistors

or set it as open drain (bit ODE register IOMUXC_SW_PAD_CTL_PAD_x_y).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,477件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

seems for unused pins one can only try to change/disable pull resistors

or set it as open drain (bit ODE register IOMUXC_SW_PAD_CTL_PAD_x_y).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,476件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick reply.

Let me confirm the meaning of your following comment.

seems for unused pins one can only try to change/disable pull resistors

What is the meaning of the pull resistors ?

I think that the pull resistor means PKE field.

Is it correct ?

Ko-hey

1,476件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes correct

Best regards

igor

0 件の賞賛
返信
1,476件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thanks !

Ko-hey

0 件の賞賛
返信