MfgTool UTP sources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MfgTool UTP sources

Jump to solution
4,235 Views
christian_neuwi
Contributor III

Where can I find the sources of the UTP daemon, i.e. the component that talks to the MfgTool in Linux user space?

 

It seems that the documentation of the MfgTool is rather outdated as many commands listed there appear to be not implemented or not functional.

Regards,

Chris.

0 Kudos
Reply
1 Solution
3,295 Views
gary_bisson
Senior Contributor III

Hi,

Here is the daemon that runs on the target:

GitHub - NXPmicro/imx-uuc: A Daemon wait for Freescale/NXP mfgtools host's command 

In case you don't have the mfgtools source code, here it is:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Regards,

Gary

View solution in original post

4 Replies
3,118 Views
daver21
Contributor I

Can someone confirm that imx-uuc is still the best option for generating a mfgtool compatible version of the os? Also are there any online resources for integrating with buildroot?

Thanks, David

0 Kudos
Reply
3,295 Views
b36401
NXP Employee
NXP Employee

You can use the links Gary provided:

https://github.com/NXPmicro/imx-uuc
https://github.com/NXPmicro/mfgtools

Have a great day,
Victor

3,296 Views
gary_bisson
Senior Contributor III

Hi,

Here is the daemon that runs on the target:

GitHub - NXPmicro/imx-uuc: A Daemon wait for Freescale/NXP mfgtools host's command 

In case you don't have the mfgtools source code, here it is:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Regards,

Gary

3,295 Views
christian_neuwi
Contributor III

Thank you, Gary!

0 Kudos
Reply