MfgTool UTP sources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,225件の閲覧回数
christian_neuwi
Contributor III

Where can I find the sources of the UTP daemon, i.e. the component that talks to the MfgTool in Linux user space?

 

It seems that the documentation of the MfgTool is rather outdated as many commands listed there appear to be not implemented or not functional.

Regards,

Chris.

0 件の賞賛
返信
1 解決策
3,285件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Here is the daemon that runs on the target:

GitHub - NXPmicro/imx-uuc: A Daemon wait for Freescale/NXP mfgtools host's command 

In case you don't have the mfgtools source code, here it is:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Regards,

Gary

元の投稿で解決策を見る

4 返答(返信)
3,108件の閲覧回数
daver21
Contributor I

Can someone confirm that imx-uuc is still the best option for generating a mfgtool compatible version of the os? Also are there any online resources for integrating with buildroot?

Thanks, David

0 件の賞賛
返信
3,285件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use the links Gary provided:

https://github.com/NXPmicro/imx-uuc
https://github.com/NXPmicro/mfgtools

Have a great day,
Victor

3,286件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Here is the daemon that runs on the target:

GitHub - NXPmicro/imx-uuc: A Daemon wait for Freescale/NXP mfgtools host's command 

In case you don't have the mfgtools source code, here it is:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Regards,

Gary

3,285件の閲覧回数
christian_neuwi
Contributor III

Thank you, Gary!

0 件の賞賛
返信